Commit c12eb3de authored by Simpson, Thomas's avatar Simpson, Thomas
Browse files

Update readme

parent 3d6ffb31
......@@ -567,4 +567,10 @@ This section describes how to run the custom Vitis-AI GStreamer plugins on the Z
# Summary
This tutorial described detailed steps used to create face and person detection GStreamer plugins using the Xilinx Vitis-AI-Library. The finished plugin source code is included in this repository in the solution directory.
\ No newline at end of file
This tutorial described detailed steps used to create face and person detection GStreamer plugins using the Xilinx Vitis-AI-Library. The finished plugin source code is included in this repository in the solution directory.
# References
- <a href="https://github.com/Xilinx/Vitis-AI/tree/master">Vitis-AI</a>
- <a href="https://github.com/Xilinx/Vitis-AI/tree/master/Vitis-AI-Library">Vitis-AI-Library</a>
- <a href="https://xterra2.avnet.com/xilinx/zcu104/zcu104-mc4-ml-example">ZCU104 FMC Quad-Camera + ML Example</a>
- <a href="https://gstreamer.freedesktop.org/">GStreamer</a>
\ No newline at end of file
Markdown is supported
0% or .
You are about to add 0 people to the discussion. Proceed with caution.
Finish editing this message first!
Please register or to comment